North American emissions compliance - Metasys - Wireless Device - ZFR-HPSST-0 Wireless Sensing System Tool

ZFR-HPSST-0 Wireless Sensing System Tool Installation Guide

Product
Network and Communications > Wireless Devices > ZFR-HPSST-0 Wireless Sensing System Tool
Document revision
C
Revision date
08/03/2023
Part number
Part No. 24-11461-00012

United States

Compliance Statement (Part 15.19)

This device complies with Part 15 of the FCC Rules. Operation is subject to the following two conditions:

  1. This device may not cause harmful interference, and
  2. This device must accept any interference received, including interference that may cause undesired operation.

Warning (Part 15.21)

Changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.

Canada

Industry Canada Statement(s)

The term IC before the certification/registration number only signifies that the Industry Canada technical specifications were met.

Le terme « IC » précédant le numéro d'accréditation/inscription signifie simplement que le produit est conforme aux spécifications techniques d'Industry Canada.