Wireless Commissioning Converter (BTCVT) - Metasys - LIT-1900345 - Field Device - BTCVT: Wireless Commissioning Converter - 10

Wireless Commissioning Converter Catalog Page

Product
Document number
LIT-1900345
Version
10
Revision date
2018-06-01

The BTCVT provides a temporary Bluetooth® connection between Metasys® system field controllers and the commissioning laptop computer. It allows technicians to commission and service the controllers over a wireless connection.

The BTCVT provides communication from the BACnet® MS/TP Field Controller (FC) Bus or the Sensor/Actuator (SA) Bus to a Bluetooth-enabled computer running the Controller Configuration Tool (CCT) software. Any MS/TP controller on an FC Bus can be commissioned by connecting to any other controller, any network sensor, or any Input/Output Module (IOM) connected to any controller on the bus, provided a FC/SA bus port is available. The BTCVT also provides CCT support for BACnet/IP controllers. However, it does not download firmware or applications to the FAC2513, FAC3613, or the BACnet/IP controllers. Only upload and commissioning of FAC2513, FAC3613, or BACnet/IP controllers is supported through BTCVT.

The 2.4 GHz Bluetooth connection allows you to be up to 10 m (33 ft) away while you commission the controller with a laptop computer and the CCT software.

Figure 1. Wireless Commissioning Converter