Selection charts - Metasys - LIT-1901153 - Wireless Device - WRG1830/ZFR183x Pro Series Wireless Field Bus System Catalog Page

WRG1830/ZFR183x Pro Series Wireless Field Bus System Catalog Page

Product
Document type
Catalog Page
Document number
LIT-1901153
Revision date
2024-12-18

For ordering information on the Wireless TEC3000s, refer to the TEC3000 Series Wireless, Stand-Alone, and Field-Selectable BACnet MS/TP or N2 Networked Thermostat Controllers Product Bulletin (LIT-12011954). For ordering information of the NSW8000 sensors, refer to the NSW8000 Series Wireless Room Sensors Product Bulletin (to be released early 2025). For more information about supported controllers, refer to the WRG1830/ZFR183x Pro Series Wireless Field Bus System Technical Bulletin (LIT-12013553).

Table 1. WRG1830/ZFR183x Pro Series Wireless Field Bus System components
Product code Description
JC-WRGKIT-0

The JC-WRGKIT-0 kit includes the following components:

  • JC-WRG1830-0: Wireless Router Gateway (WRG)
  • JC-ZFR1831-0: ZFR1831Pro Wireless Router
  • ACC-WIFIKIT-0DU: USB Wi-Fi Dongle

Order one for each wireless network.

JC-ZFR1831-0

The JC-ZFR1831-0 kit includes the following:

  • One ZFR1831 Pro Wireless Router

Order one for each field controller or one for each repeater that you require.

Table 2. Optional accessories
Product code Description
ZFR-CBLEXT-0

The optional ZFR-CBLEXT-0 includes:

  • One ZFR-CBLEXT-1.
  • One female to female RJ12 coupler to connect multiple cables.
Note: The ZFR1831 Router/Repeater physical cabling can be extended up to 100 ft maximum.
Note: The ZFR1831 Router/Repeater physical cabling termination can be either RJ12 or terminal block.
ZFR-CBLEXT-1

The optional ZFR-CBLEXT-1 includes:

  • One 10 ft RJ12 terminated cable to connect the ZFR1831 Pro Router/Repeater to the controller or the WRG1830.
ZFR-HPSST-0

The ZFR-HPSST-0 includes:

  • One ZFR1831 Router
  • One ZFR-SSTBAT-0 Battery Pack
  • Two magnets to temporarily mount devices

The ZFR-HPSST-0 is a selectable 10 mW/100 mW wireless survey tool. Use this tool to verify the expected signal strength and performance of ZFR183x wireless devices after installation.

Note: Use any JC-ZFR1831-0 as an HPSST simply by connecting the battery case (ZFR-HPSST-0) and moving the battery jumper.
Important: Two ZFR-HPSST-0 tools are required to perform signal strength testing. It is recommended that each installation team have a pair of ZFR-HPSST tools.
ZFR-SSTBAT-0 The ZFR-SSTBAT-0 is a replacement or spare battery case with connector for use with the ZFR1831 Router when used as a Survey tool.
  • Includes two 1.5VDC, AA Alkaline batteries
AA alkaline battery, 1.5 VDC Replacement battery for WRZ Series Sensors, purchase locally.
Note: The WRZ Sensor ships with quantity two alkaline batteries. Longer battery life can be achieved if locally replaced with lithium batteries.
ACC-PWRKIT-1A24

The optional kit includes:

  • One WRG 110/220 VAC Power Supply for North America
Note: The Wireless Router Gateway (WRG) supports 24 VAC input by default
ACC-WIFIKIT-0DU This ACC-WIFIKIT-0DU kit is a replacement or spare Wireless Router Gateway (WRG) Wi-Fi Dongle for North America
JC-WRG1830-0 The WRG1830-0 is a replacement or spare WRG Gateway. The kit includes:
  • One WRG1830-0 Gateway