Set the PAN IDs on Your ZFR Pro Devices - Metasys - LIT-12012319 - MS-WNC1800-0S - MS-WNC1820-0A - MS-WNC1820-0B - MS-WNC1823-0A - MS-WNC1823-0B - MS-ZFR1820-0 - MS-ZFR1821-0 - MS-ZFR1821-0B - MS-ZFR1822-0 - MS-ZFR1822-0B - MS-ZFR1823-0 - WNC-120V-PS-0 - WNC-24V-PS-0 - ZFR-24V-PS-0 - ZFR-CBLEXT-0 - ZFR-WallCover - Bulb controller - FX-ZFR182x Pro Series Wireless Field Bus System

WNC1800/ZFR182x Pro Series Wireless Field Bus System Quick Reference Guide

Product
Network and Communications > Wireless Devices > FX-ZFR182x Pro Series Wireless Field Bus System
Document type
Reference Guide
Document number
LIT-12012319
Revision date
01/02/2017

Set the PAN ID DIP switches on the ZFR Pro Coordinator Radio, ZFR Pro Router/Repeater and WRZ Sensors. See Figure 1.

Notes:

  • Select PAN Addresses that are unique within the site.
  • All devices on the wireless network need to have the same PAN Offset.
  • All the Field Controllers' MS/TP Addresses and the TECs' BACnet Addresses must be unique within the same PAN. See Figure 2..
    Figure 1. Sample DIP Switch Settings

    Figure 2. TEC Network Setup and Configuration Menu