Discover the Field Controllers on Your Network - Metasys - LIT-12012319 - Wireless Device - WNC: Wireless Network Coordinator/Gateway

WNC1800/ZFR182x Pro Series Wireless Field Bus System Quick Reference Guide

Brand
Metasys
Product name
WNC: Wireless Network Coordinator/Gateway
Document type
Reference Guide
Document number
LIT-12012319
Revision date
2017-02-01
Language
English

Once the WEFC's are powered on and begin communication with the WNC1800 Gateway, the Number of Online Devices will increase until all WEFC's on your network are discover. If a WEFC stops communicating for any reason, the Number of Online devices will decrease and the Number of Offline devices will increase.

Note: It is not usually necessary to use the Rediscover Devices button, but this action may be required if a WEFC has been permanently removed from the PAN, if alarms and status indications do not self-clear, firmware has been updated, or new applications have been downloaded to the controllers.
Figure 1. WNC Home Page

Once devices are recognized by the WNC Gateway, you can view and edit the settings on the connected devices by accessing them through the Device List. See the Related Literature section in this document to find the literature specific to the device you are setting up.