Complete the Network Setup - Metasys - LIT-12012319 - Wireless Device - WNC: Wireless Network Coordinator/Gateway

WNC1800/ZFR182x Pro Series Wireless Field Bus System Quick Reference Guide

Brand
Metasys
Product name
WNC: Wireless Network Coordinator/Gateway
Document type
Reference Guide
Document number
LIT-12012319
Revision date
2017-02-01
Language
English

On the Network Setup Screen shown below, the Wireless Field Bus Network address, BACnet Device Object Identifier, and the BACnet IP Network address must be unique. One simple way to make the Wireless Field Bus Network address, BACnet Device Object Identifier, and the BACnet IP Network address is unique is to set it to the PAN ID of the attached coordinator. Other methods can also be used if appropriate for the site.

If you add the WNC Gateway and associated devices to a network that has a Supervisory Controller, the Routing Mode field on the WNC Home Page must be set to Enabled.

Notes:

  • Once you make these changes, you must set the Commit Changes and Reset field to True; then the WNC Gateway resets and uses the new settings.
    Figure 1. WNC Network Setup