Wiring the H-Link Network - Metasys - Part No. 24-10143-1183 - SI-VRFCBN02-0Sx - Gateway/Router - VRF Smart Gateway - Release 1.2.1

VRF Smart Gateway Installation Guide

Product
Network and Communications > Gateways and Routers > VRF Smart Gateway
Document type
Installation Guide
Document number
Part No. 24-10143-1183
Document revision
Rev. H
Version
Release 1.2.1
Revision date
2022-04-12

To wire the H-Link Network of the VRF Smart Gateway:

Note: The use of 18 AWG/2-wire/stranded/shielded/copper cable is required.
  1. Connect the two H-Link cable wires to the left terminals indicated in Figure 1.
  2. If the VRF Smart Gateway is connected at an intermediate position of the H-Link network as opposed to the end of the network segment, use the right terminals shown in Figure 1 to continue the H-Link network.
Figure 1. H-Link cable insert position

To insert or remove the H-Link cable wires:

  1. Push the orange tabs using a small, flat screwdriver or similar tool as indicated in Figure 2.
  2. Insert or remove the wire and release the tab.
Figure 2. Inserting or Removing the H-Link Cable Wires