Wiring Consideration and Guidelines - Metasys - Part No. 24-10143-1183 - SI-VRFCBN02-0Sx - Gateway/Router - VRF Smart Gateway - Release 1.2.1

VRF Smart Gateway Installation Guide

Product
Network and Communications > Gateways and Routers > VRF Smart Gateway
Document type
Installation Guide
Document number
Part No. 24-10143-1183
Document revision
Rev. H
Version
Release 1.2.1
Revision date
2022-04-12

Observe the following guidelines when wiring the VRF Smart Gateway:

  • Do not allow the VRF Smart Gateway to hang from a cable connection.

  • Provide some slack in the cable between the VRF Smart Gateway and the controller or other device to which you are connecting.