VRF Smart Gateway LED Designations and Descriptions - Metasys - Part No. 24-10143-1183 - SI-VRFCBN02-0Sx - Gateway/Router - VRF Smart Gateway - Release 1.2.1

VRF Smart Gateway Installation Guide

Product
Network and Communications > Gateways and Routers > VRF Smart Gateway
Document type
Installation Guide
Document number
Part No. 24-10143-1183
Document revision
Rev. H
Version
Release 1.2.1
Revision date
2022-04-12
Part number
24-10143-1183
Table 1. LED Designations and Descriptions

LED Name

Color

Normal

Descriptions/Other Conditions

Power

Green

On solid (no flashing)

Off = No power

On solid = Power supplied by primary voltage

Fault

Red

Off

Off = No faults/normal operation

On solid = Missing hardware, missing software, operating system has not yet initialized, or reset is in progress.

Slow Flicker (one blink per second) = Software update in progress

Medium Flicker (two blinks per second) = Startup sequence

Fast Flicker (five blinks per second) = Fault

H-Link Bus

Green

On solid

Off = No data transmitting

Fast Flicker = Software update of second processor

Slow Flicker (one blink per second) = Discovering VRF devices

On solid = Discovery complete

Ethernet

Green

On solid

Off = Communication not established

On solid = Communication established

Flicker = Data transmission

Wi-Fi

Yellow

On solid

Off = No Wi-Fi signal or no devices currently connected over Wi-Fi

Wi-Fi strength is indicated by the number of LEDs that are lit, with one lit LED indicating weak wireless signal strength (between 1% and 49%) and three lit LEDs indicating excellent wireless signal strength (at least 75%).