Ethernet Port - Metasys - Part No. 24-10143-1183 - SI-VRFCBN02-0Sx - Gateway/Router - VRF Smart Gateway - Release 1.2.1

VRF Smart Gateway Installation Guide

Product
Network and Communications > Gateways and Routers > VRF Smart Gateway
Document type
Installation Guide
Document number
Part No. 24-10143-1183
Document revision
Rev. H
Version
Release 1.2.1
Revision date
2022-04-12
Part number
24-10143-1183

The Ethernet port on the VRF Smart Gateway is an 8-pin RJ-45 jack. The maximum allowable cable length is 328 ft (100 m). The Ethernet port on the VRF Smart Gateway connects to the BAS by using an Ethernet switch or similar networking equipment.