Update Software - Metasys - Part No. 24-10143-1183 - SI-VRFCBN02-0Sx - Gateway/Router - VRF Smart Gateway - Release 1.2.1

VRF Smart Gateway Installation Guide

Brand
Metasys
Product name
VRF Smart Gateway
Document type
Installation Guide
Document number
Part No. 24-10143-1183
Document revision
Rev. H
Version
Release 1.2.1
Revision date
2022-04-12
Language
English
Important: The VRF Smart Gateway software update process must be followed per the sequence identified below. You cannot upgrade a VRF Smart Gateway already in the field running firmware earlier than V1.2.0.266 directly to V1.2.1.54. The MUT tool must be used.
Note: This updated document applies to the V1.2.1.54.
Important: VRF Smart Gateway units already in the field must follow the following update process:
  • If the VRF Smart Gateway version is at an earlier version than 1.1.0.833/.834, upgrade the Gateway to 1.1.0.833/.834 at minimum using the standard software upgrade process from the VRF Smart Gateway UI.
  • If the VRF Smart Gateway is at 1.1.0.833/.834, use the MUT tool to upgrade the Gateway to the 1.2.0.266 build. The MUT Software Update Tool is required because there are OS migration and security fixes in the VRF Smart Gateway V1.2.0.266 software release. The standard software upgrade from a VRF Smart Gateway UI procedure is not possible.
  • If the VRF Smart Gateway is at 1.2.0.266, then upgrade the Gateway to 1.2.1.54 by using the standard software upgrade process from VRF Smart Gateway UI.
Note: For more information on software upgrade using the MUT, refer to the VRF Smart Gateway MUT User Guide (LIT-12013562). For more information about software update from the VRF Smart Gateway UI, refer to the VRF Smart Gateway Users Guide (LIT-12012385).