Mounting - Metasys - Part No. 24-10143-1183 - SI-VRFCBN02-0Sx - Gateway/Router - VRF Smart Gateway - Release 1.2.1

VRF Smart Gateway Installation Guide

Product
Network and Communications > Gateways and Routers > VRF Smart Gateway
Document type
Installation Guide
Document number
Part No. 24-10143-1183
Document revision
Rev. H
Version
Release 1.2.1
Revision date
2022-04-12
Part number
24-10143-1183

We recommend mounting the unit either vertically (upright and flush) or horizontally (sideways and flush). This flexibility allows the unit to be mounted in a way that minimizes spacial constraints and maximizes placement options for optimal wireless signal strength.

The unit should be mounted in such a way that labels can be read if they are visible. For example, do not mount the unit upside down, which puts the labels upside down.