Wiring the H-Link Network - Metasys - Part No. 24-10143-1183 - SI-VRFCBN02-0Sx - Gateway/Router - VRF Smart Gateway

VRF Smart Gateway Installation Guide

Product
Network and Communications > Gateways and Routers > VRF Smart Gateway
Document number
Part No. 24-10143-1183
Document revision
F
Revision date
2020-04-23
Part number
24-10143-1183

To wire the H-Link Network of the VRF Smart Gateway:

  • Connect the two H-Link cable wires to the left terminals indicated in the following figure.
  • If the VRF Smart Gateway is connected at an intermediate position of the H-Link network as opposed to the end of the network segment, use the right terminals shown in the following figure to continue the H-Link network.
Figure 1. H-Link Cable Insert Position

To insert or remove the H-Link cable wires:

  • Push the orange tabs using a small, flat screwdriver or similar tool as indicated in the following figure.
  • Then, insert or remove the wire and release the tab.
Figure 2. Inserting or Removing the H-Link Cable Wires