You can perform two levels of factory reset on the VRF Smart Gateway, as shown in Table 1.
The reset button is on the side of the device, and it is embedded into the VRF Smart Gateway housing so that it cannot be activated by accident. To reach the reset button, use a paper clip, pin, or similar tool.
|
Reset Function |
Reset Operation |
|---|---|
|
Reset Wi-Fi (SSID and passphrase) and Ethernet Settings |
|
|
Reset all unit settings to Factory Defaults (resets all unit settings, including user profiles) |
|
- For information on LED designations and flicker behavior, see Table 1.
- If you press the reset button, anyone connected to the VRF Smart Gateway is disconnected.
- If you press the reset button for more than 9 seconds, the reset operation is cancelled.
- If you do not press the reset button a second time within 5 seconds of releasing it, the reset operation is cancelled.
- If a fault condition already exists, the reset button is disabled.