Configuring the IP Settings for the BAS - Metasys - Part No. 24-10143-1183 - SI-VRFCBN02-0Sx - Gateway/Router - VRF Smart Gateway

VRF Smart Gateway Installation Guide

Product
Network and Communications > Gateways and Routers > VRF Smart Gateway
Document number
Part No. 24-10143-1183
Document revision
F
Revision date
2020-04-23
Part number
24-10143-1183

About this task

You must set the IP address, Subnet Mask, and Default Gateway for the VRF Smart Gateway to communicate with the BAS's integration device, such as the Metasys NAE or the FX80.

Procedure

  1. In the gateway UI, navigate to Settings > Ethernet.
  2. Choose one of the following options for IP settings, depending on customer preferences, and whether or not the building network supports DHCP :
    1. To use DHCP, in the Auto DHCP Configure list, select On.
    2. To use a fixed IP address, in the Auto DHCP Configure list, select Off. A Static IP address, Subnet Mask, and Default Gateway must be decided on and entered into the appropriate fields.
  3. Optional: For best results, add the gateway and the NAE on the same IP subnet. If the gateway and NAE are not on the same IP subnet, you may need to use a new release 1.1 feature called BBMD.
  4. Leave the DNS settings blank.
  5. Click Save. You are prompted to restart the gateway now or postpone. If you are configuring the BACnet settings, you can postpone the restart until after they are configured. If you have configured both the IP settings and the BACnet settings, restart now.