The following table lists the available BACnet points for the VRF indoor units (IDUs) as exposed by the VRF Smart Gateway.
BACnet Instance Number |
Object Name |
Object Description |
Object Type |
Contents of Information |
|||||
---|---|---|---|---|---|---|---|---|---|
4 |
UNIT-CAP |
Indoor Unit Capacity Code |
AI |
Value |
0 to 255 |
||||
5 |
UNITEN-MODE |
Unit Enable Mode |
BO |
Setting |
Shutdown |
Enable |
– |
– |
– |
6 |
SYSTEM-MODE |
Command System Mode |
MO |
Setting |
Cool |
Dry |
Fan |
Heat |
Auto |
7 |
HtClg-REQ |
Heat/Cool Required |
BI |
Status |
False |
True |
– |
– |
– |
8 |
SF-SPEED-C |
Commanded Supply Fan Speed |
MO |
Setting |
Low |
Medium |
High |
Auto |
– |
9 |
EXPV-% |
Expansion Valve Position |
AI |
Value |
0.0% to 100.0% |
||||
10 |
LIQ-PIPE-T |
Liquid Pipe Temperature |
AI |
Value |
-50°C to 99°C (-58°F to 210°F) |
||||
11 |
GAS-PIPE-T |
Gas Pipe Temperature |
AI |
Value |
-50°C to 99°C (-58°F to 210°F) |
||||
12 |
RA-T |
Return Air Temperature |
AI |
Value |
-50°C to 99°C (-58°F to 210°F) |
||||
13 |
DA-T |
Discharge Air Temperature |
AI |
Value |
-50°C to 99°C (-58°F to 210°F) |
||||
14 |
DIFF-T |
Coil Differential Temperature |
AI |
Value |
-127°C to 127°C (-196°F to 260°F) |
||||
15 |
ZN-SP |
Zone Temperature Setpoint |
AO |
Setting |
17°C to 30°C (62°F to 86°F) |
||||
16 |
RZN-T 1 |
Remote Zone Temperature |
AI |
Value |
-50°C to 99°C (-58°F to 210°F) |
||||
17 |
COMP to REQ |
Requested Compressor Speed |
AI |
Value |
0 Hz to 255 Hz |
||||
18 |
UNIT-STOP-CODE |
Unit Stop Code |
AI |
Value |
0 to 255 For information about individual code numbers, refer to the VRF equipment service manual. |
||||
19 |
ALARM-CODE |
Alarm Code |
AI |
Value |
0 to 255 For information about individual code numbers, refer to the VRF equipment service manual. |
||||
20 |
RMT-OPT |
Optional Room Thermostat |
BI |
Status |
False |
True |
– |
– |
– |
21 |
DEFROST-S |
Defrost Status |
BI |
Status |
False |
True |
– |
– |
– |
22 |
REM-CON |
Remote Control Connected |
BI |
Status |
False |
True |
– |
– |
– |
23 |
SF-S |
Supply Fan Status |
BI |
Status |
Off |
On |
– |
– |
– |
24 |
ALARM-S |
Unit Alarm Status |
BI |
Status |
Normal |
Alarm |
– |
– |
– |
25 |
SYSTEM-S |
Actual System Mode |
MI |
Status |
Cool |
Dry |
Fan |
Heat |
– |
26 |
SF-SPD |
Actual Supply Fan Speed |
MI |
Status |
Low |
Medium |
High |
– |
– |
27 |
ZN-T 2 |
Zone Temperature |
AI |
Value |
-50°C to 99°C (-58°F to 210°F) |
||||
28 |
FILT-S |
Filter Status |
BI |
Status |
Clean |
Dirty |
– |
– |
– |
29 |
FILT-S-RESET |
Filter Status Reset |
BO |
Setting |
Clean |
Dirty |
– |
– |
– |
30 |
UNIT-LO |
Unit Lockout |
BO |
Setting |
Unlock |
Lock |
– |
– |
– |
31 |
FANCMD-LO |
Fan Command Lockout |
BO |
Setting |
Unlock |
Lock |
– |
– |
– |
32 |
SYSMODE-LO |
System Mode Lockout |
BO |
Setting |
Unlock |
Lock |
– |
– |
– |
33 |
ZNSP-LO |
Zone Temperature Setpoint Lockout |
BO |
Setting |
Unlock |
Lock |
– |
– |
– |
34 |
FANSPD-LO |
Fan Speed Lockout |
BO |
Setting |
Unlock |
Lock |
– |
– |
– |
35 |
LOUVER-LO |
Louver Position Lockout |
BO |
Setting |
Unlock |
Lock |
– |
– |
– |
The following table lists the IDU multi-state values for SYSTEM-MODE and SYSTEM-S.
State Value |
State String |
---|---|
1 |
Cool |
2 |
Dry |
3 |
Fan |
4 |
Heat |
5 |
Auto |
The following table lists the IDU multi-state values for SF-SPEED-C and SF-SPD.
State Value |
State String |
---|---|
1 |
Low |
2 |
Med |
3 |
High |
4 |
Auto |
The following table lists the available BACnet points for the VRF outdoor units (ODUs) as exposed by the VRF Smart Gateway.
BACnet Instance Number |
Object Name |
Object Description |
Object Type |
Contents of Information |
|||
---|---|---|---|---|---|---|---|
3 |
ALARM-CODE |
Alarm Code |
AI |
Value |
0 to 255 For information about individual code numbers, refer to the VRF equipment service manual. |
||
6 |
SYSTEM-MODE |
System Mode |
MI |
Status |
Heat |
Cool |
Auto |
7 |
SYSTEM-S |
System Status |
MI |
Status |
Several Values (See the Following Tables for Multi-State Information) |
||
8 |
HX-STATE |
Heat Exchanger State |
MI |
Status |
Several Values (See the Following Tables for Multi-State Information) |
||
9 |
INV-STATE |
Inverter State |
MI |
Status |
Several Values (See the Following Tables for Multi-State Information) |
||
10 |
FAN-STATE |
Fan Controller State |
MI |
Status |
Several Values (See the Following Tables for Multi-State Information) |
||
11 |
INV-HRS |
Inverter Compressor 1 Runtime |
AI |
Value |
0 Hours to 655,350 Hours |
||
12 |
COMP-HRS |
Compressor 2 Runtime |
AI |
Value |
0 Hours to 655,350 Hours |
||
13 |
INV-FREQ |
Inverter Compressor Frequency |
AI |
Value |
0 Hz to 255 Hz |
||
14 |
TOTAL-FREQ |
Total Frequency |
AI |
Value |
0 Hz to 65,535 Hz |
||
15 |
FAN-% |
Outdoor Fan Output |
AI |
Value |
0% to 100% |
||
16 |
EXPV-% |
Expansion Valve Position |
AI |
Value |
0% to 100% |
||
17 |
BYPEXPV-% |
Bypass Expansion Valve Position |
AI |
Value |
0% to 100% |
||
18 |
DISCH-P |
Discharge Pressure |
AI |
Value |
0 psi to 3,698.5 psi |
||
19 |
SUCT-P |
Suction Pressure |
AI |
Value |
0 psi to 369.8 psi |
||
20 |
OA-T |
Outside Air Temperature |
AI |
Value |
-50°C to 99°C (-58°F to 210°F) |
||
21 |
INV2ND-A |
Inverter Compressor Secondary Current |
AI |
Value |
0 A to 127.0 A |
||
22 |
INVPRI-A |
Inverter Compressor Primary Current |
AI |
Value |
0 A to 127.0 A |
||
23 |
COMP2-A |
Compressor 2 Current |
AI |
Value |
0 A to 127.0 A |
||
24 |
INVTOP-T |
Inverter Compressor Top Temperature |
AI |
Value |
0°C to 99°C (32°F to 210°F) |
||
25 |
COMP2TOP-T |
Compressor 2 Top Temperature |
AI |
Value |
0°C to 99°C (32°F to 210°F) |
||
26 |
PROT-CODE |
Protection Code |
MI |
Status |
Several Values (See the Following Tables for Multi-State Information) |
||
27 |
DEFROST-S |
Defrost Status |
BI |
Status |
Off |
On |
– |
28 |
EMERGRUN-S |
Emergency Run Status |
BI |
Status |
Off |
On |
– |
29 |
INV-S |
Inverter Status |
BI |
Status |
Stop |
Run |
– |
30 |
FAN-S |
Fan Status |
BI |
Status |
Stop |
Run |
– |
The following table lists the ODU multi-state values for SYSTEM-MODE.
State Value |
State String |
---|---|
1 |
Heat |
2 |
Cool |
3 |
Auto |
The following table lists the ODU multi-state values for SYSTEM-S.
State Value |
State String |
---|---|
1 |
Thermo off |
2 |
Pump down |
3 |
SW on start |
4 |
Thermo on start |
5 |
After defrost |
6 |
Start control 1 |
7 |
Start control 2 |
8 |
Normal |
9 |
Oil return |
10 |
Defrost ready 1 |
11 |
Defrost ready 2 |
12 |
Differential pressure control |
13 |
Defrost |
The following table lists the ODU multi-state values for HX-STATE.
State Value |
State String |
---|---|
1 |
Evaporator Mode Low Pressure |
2 |
Condenser Mode High Pressure |
3 |
Evaporator Mode |
4 |
Condenser Mode |
The following table lists the ODU multi-state values for INV-STATE and FAN-STATE.
State Value |
State String |
---|---|
1 |
Normal stop |
2 |
Fault |
3 |
Over current |
4 |
Fin temp |
5 |
Electronic thermal |
6 |
Undervoltage |
7 |
Overvoltage |
8 |
Communication error |
9 |
Current sensor abnormality |
10 |
Instantaneous power failure |
12 |
MPU reset |
13 |
Earth fault voltage |
14 |
Phase loss |
16 |
Driving prohibited area |
17 |
Fan controller retry |
18 |
Control abnormality |
21 |
Loss of synchronism |
24 |
Normal acceleration |
25 |
Normal deceleration |
26 |
Constant speed |
27 |
Overload after the acceleration |
28 |
Overload after the deceleration |
29 |
Overload after constant speed |
30 |
Power supply unbalance |
31 |
Power supply phase loss |
The following table lists the ODU multi-state values for PROT-CODE.
State Value |
State String |
---|---|
1 |
Pressure ratio |
2 |
Pd rise prevention |
3 |
Current protection |
4 |
INV module temp rise prevent |
5 |
Compressor top overheat prevent |
6 |
Ps drop or rise prevention |
9 |
Pd drop prevention |
10 |
Current demand |
13 |
Ps rise prevention |