Overview - Metasys - LIT-12011931 - MS-MBUSN89-0 - TL-NIE-DVD - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - VMD Generator Express - 10

VMD Generator Express Application Note

Product
Building Automation Systems > Building Automation Systems > VMD Generator Express
Document number
LIT-12011931
Version
10
Revision date
2017-06-01

The NIEx9 integration engine uses the VMD resource files created by the VGE tool to allow communication between Modbus devices and the Metasys building management system. These resource files include the Modbus registers and the rules used to treat the data coming from Modbus devices. In addition to VMD file creation, the intuitive user interface of VGE tool lets you:

  • track file versions and revision history of each VMD file
  • create temporary VMD files to serve as templates
  • export a table of all points for use with Microsoft Excel