Verifying the VMD History - Metasys - LIT-12011931 - MS-MBUSN89-0 - TL-NIE-DVD - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - VMD Generator Express - 10

VMD Generator Express Application Note

Product
Building Automation Systems > Building Automation Systems > VMD Generator Express
Document type
Application Note
Document number
LIT-12011931
Version
10
Revision date
01/06/2017

About this task

You can find the most recent history entry in the history table of the Metasys interface.

In order to verify the VMD history, create a binary input point called VERSION by following these steps:

Procedure

  1. In the Insert Point Wizard, select the parent item for your new item.
    Figure 1. Insert Dummy Point to Show the Version (1)

  2. Select the type of field point you want to create.
    Figure 2. Insert Dummy Point to Show the Version (2)

  3. Select a unique field point identification.
    Figure 3. Insert Dummy Point to Show the Version (3)

    Figure 4. Version Information in Metasys Interface