About this task
You can manipulate data in the Points table by using the Table Editor. For example, you can perform a global search and replace on any text that appears in any column of the Points table.
Procedure
-
Select View > Table Editor, or click the Table Editor toolbar button (Figure 1).
Figure 1. Table Editor Toolbar Icon
The Table Editor window appears (Figure 2).
Figure 2. Table Editor
- In the Column Selection drop-down box, select which column you want to use for the action. You can select from the following columns: Unique ID, Description, Units, States Text, Display Precision, Function, Address, Data Type, Mathematical Function, Slope (m), Intercept (q), and Comment. The Action and Action Range fields pre-populate for you.
- In the Action drop-down box, select Find and Replace or Replace All.
- In the Action Range drop-down box, select Selected Cells or All Cells.
- In the Find field, make an appropriate entry depending on what type of data you are looking for. Either type in the value or select it from the drop-down box.
- In the Replace field, make an appropriate entry depending on what type of data you are replacing. Either type in the value or select it from the drop-down box.
- In the Append field, make an appropriate entry if one is required.
-
Click Execute. The changes are made to the Points table, and a Results
Report appears to summarize what was changed (Figure 3).
Figure 3. Example of Results Report