Saving a File - Metasys - LIT-12011931 - MS-MBUSN89-0 - TL-NIE-DVD - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - VMD Generator Express - 10

VMD Generator Express Application Note

Product
Building Automation Systems > Building Automation Systems > VMD Generator Express
Document number
LIT-12011931
Version
10
Revision date
01/06/2017

About this task

Procedure

  1. Select File > Save As, or click the Save toolbar button.
  2. In the Save File dialog box, browse to the desired folder.
  3. Type the file name and use the Save as type drop-down list to save the file as either a VMD or VMT file.
  4. Click Save.