Deleting a Row - Metasys - LIT-12011931 - MS-KNXN89-0 - MS-MBUSN89-0 - MS-MODBUSN89-0 - MS-NIE2910-0 - MS-NIE2916-0 - MS-NIE2920-0 - MS-NIE2926-0 - MS-NIE2960-0 - MS-NIE2966-0 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE4910-2 - MS-NIE4920-2 - MS-NIE5920-2 - MS-NIE5960-2 - MS-NIE89SW-0 - MS-NIE89SW-6 - TL-NIE-DVD - Bulb controller - VMD Generator Express - 10

VMD Generator Express Application Note

Product
Building Automation Systems > Building Automation Systems > VMD Generator Express
Document type
Application Note
Document number
LIT-12011931
Version
10
Revision date
01/06/2017

About this task

You can delete single or multiple rows from the points tab.

Procedure

  1. Select the row or rows you want to delete.
    Note: To select multiple rows, use SHIFT to select a range of rows and hold down CTRL to select individual rows.
  2. Select Edit > Delete Rows, or click the Delete Rows toolbar button.
    Figure 1. Delete Rows Toolbar Icon

  3. Click Yes to delete the row.

    The selected row is removed from the Points tab (Figure 2).

    Figure 2. Row Removed