Creating a New File - Metasys - LIT-12011931 - MS-MBUSN89-0 - TL-NIE-DVD - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - VMD Generator Express - 10

VMD Generator Express Application Note

Product
Building Automation Systems > Building Automation Systems > VMD Generator Express
Document number
LIT-12011931
Version
10
Revision date
2017-06-01

About this task

You create VMD or VMT files for integration between NIEx9 devices and the Modbus protocol.

You can begin creating a new file in one of two ways:
  • Select File > New.
  • Click the New toolbar button (Figure 1).
Figure 1. New Toolbar Button

The Points tab and points headings appear and you can begin adding rows for your file data. For more information on adding rows, see Adding Rows.
Figure 2. Point Headers Added