Adding and Removing the Gateway Formula - Metasys - LIT-12011931 - MS-MBUSN89-0 - TL-NIE-DVD - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - VMD Generator Express - 10

VMD Generator Express Application Note

Product
Building Automation Systems > Building Automation Systems > VMD Generator Express
Document type
Application Note
Document number
LIT-12011931
Version
10
Revision date
01/06/2017

About this task

Files with Gateway capabilities are used to access the Modbus devices and supply information in a modular and repetitive way. Formula and parameters are used to move the pointer at the desired memory location.

Procedure

  1. Select Edit > Add Gateway Formula.
    Figure 1. Gateway Formula

    The Gateway Formula is added at the top of the table (Figure 2).

    Figure 2. Gateway Formula Added to Points Tab

  2. Click Formula in the Unique ID column to add the address and set the pointer.
  3. To remove the Gateway Formula, select Edit > Remove Gateway Formula.