Adding Rows - Metasys - LIT-12011931 - MS-MBUSN89-0 - TL-NIE-DVD - MS-NIE2920-0 - MS-NIE89SW-6 - MS-NIE2966-0 - MS-KNXN89-0 - MS-NIE2910-0 - MS-NIE5920-2 - MS-NIE2960-0 - MS-NIE5960-2 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE2916-0 - MS-NIE2926-0 - MS-NIE4920-2 - MS-NIE4910-2 - MS-MODBUSN89-0 - MS-NIE89SW-0 - Bulb controller - VMD Generator Express - 10

VMD Generator Express Application Note

Product
Building Automation Systems > Building Automation Systems > VMD Generator Express
Document number
LIT-12011931
Version
10
Revision date
01/06/2017

About this task

Once you have opened a new file, you add rows to specify file functions. For more information on available point parameters, see Table 1.

Procedure

  1. Select Edit > Add Row, or click the Add Row toolbar button (Figure 1).
    Figure 1. Add Row Toolbar Icon

    A Vendor Configuration Data (VCD) row appears under the points headings (Figure 2).

    Figure 2. Rows Added

  2. Add as many rows as needed to create your file.
  3. Once you have added the desired number of rows, use the drop-down lists and type the required points data into each VCD row.