File Menu - Metasys - LIT-12011931 - MS-KNXN89-0 - MS-MBUSN89-0 - MS-MODBUSN89-0 - MS-NIE2910-0 - MS-NIE2916-0 - MS-NIE2920-0 - MS-NIE2926-0 - MS-NIE2960-0 - MS-NIE2966-0 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE4910-2 - MS-NIE4920-2 - MS-NIE5920-2 - MS-NIE5960-2 - MS-NIE89SW-0 - MS-NIE89SW-6 - TL-NIE-DVD - Bulb controller - VMD Generator Express - 10

VMD Generator Express Application Note

Product
Building Automation Systems > Building Automation Systems > VMD Generator Express
Document type
Application Note
Document number
LIT-12011931
Version
10
Revision date
01/06/2017
Figure 1. File Menu

Table 1. File Menu Descriptions

Menu Item

Description

New

Clears the main window and allows you to create a new file.

Open

Lets you browse to a saved file.

Save As

Lets you name and save a new file.

Close

Closes the active tab.

Export

Exports a subset of rows from one integration to another. You save the file as a vendor model export file (.vme extension) for import into another integration.

Import

Imports a subset of rows from one integration to another. You import an existing vendor model export file (.vme extension) into the integration.

Export Points Mapping Table

Exports the Points Mapping Table to a comma-separated value (CSV) file for use with Microsoft® Excel.

Copy Points Table for Application Notes

Copies the Points Table for creation of application notes. This menu item is reserved for System Integration Services (SIS) Europe.

Exit

Closes the VGE Tool.