History Tab - Metasys - LIT-12011931 - MS-KNXN89-0 - MS-MBUSN89-0 - MS-MODBUSN89-0 - MS-NIE2910-0 - MS-NIE2916-0 - MS-NIE2920-0 - MS-NIE2926-0 - MS-NIE2960-0 - MS-NIE2966-0 - MS-NIE3910-2 - MS-NIE3920-2 - MS-NIE4910-2 - MS-NIE4920-2 - MS-NIE5920-2 - MS-NIE5960-2 - MS-NIE89SW-0 - MS-NIE89SW-6 - TL-NIE-DVD - Bulb controller - VMD Generator Express - 10

VMD Generator Express Application Note

Product
Building Automation Systems > Building Automation Systems > VMD Generator Express
Document type
Application Note
Document number
LIT-12011931
Version
10
Revision date
01/06/2017

The History tab lists all actions made to the VMD file. Each row displays the date and time of the file creation, the user that created or modified the file, and comments added by the user.

Figure 1. VMD Generator Express History

When a file is saved, you must enter a comment that is stored in the version record. An option to clear this history is available and must be initiated at the end of the debugging phase of the file.

Figure 2. Version Comments