VMD — Vendor Model Definition File |
VMT — Vendor Model Temporary File |
---|---|
The VMD file interfaces with the NIEx9 device and includes registers and rules that must be applied. |
The VMT file is used to temporarily save the project. |
This file requires a user version comment when saved. |
The file does not require a user version comment when saved. |
When a VMD file is saved, the file name is locked and cannot be changed. |
This type of file cannot be used as a driver inside the NIEx9 resource file. |
If the file is renamed, it is considered invalid when loaded into the NIEx9 as a resource file. |
VMT files can be opened and created only if you have a Create license. |
Note: When a VMD file is saved with a modify-only license, you can modify some fields.
However, the following modifications are prohibited:
|
If you create a VMD file similar to the original, the new VMD file uses the VMT file as a base. VMT files can also be used to recreate the same file, but introducing modifications, such as adding a point, are not allowed. |