Modular port - Metasys - MS-VMA1832-x - MS-VMA1826-x - Field Device - VMA18 VAV Modular Assembly

VMA1826/1832 VAV Controller Installation Guide

Product
Variable Air Volume > Modular Assemblies > VMA18 VAV Modular Assembly
Document revision
K
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-373

The modular (TSTAT) port on the face of the VMA ( Figure 1 ) is an RJ-45, 8-position modular jack used to connect your new or existing sensor to the VMA using one of the two included adapters. Refer to the Sensor Replacement section in the N2 VMA Application Note (LIT-12011829 ).

Figure 1. Pin number assignments for the modular port on VMA 18 Controllers