Input and Output terminals - Metasys - MS-VMA1832-x - MS-VMA1826-x - Field Device - VMA18 VAV Modular Assembly

VMA1826/1832 VAV Controller Installation Guide

Product
Variable Air Volume > Modular Assemblies > VMA18 VAV Modular Assembly
Document revision
K
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-373

The input spade terminals are located on the side of the VMA near the N2/FC Bus terminal block. The output spade terminals are located on the opposite side of the controller near the power supply spade terminals. See Table 1 for more information.