VMA terminals and bus ports - Metasys - MS-VMA1826-x - MS-VMA1832-x - Field Device - VMA18 VAV Modular Assembly

VMA1826/1832 VAV Controller Installation Guide

Product
Variable Air Volume > Modular Assemblies > VMA18 VAV Modular Assembly
Document type
Installation Guide
Document revision
K
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-373

See Figure 1 for input and output terminal and bus port locations on the VMA18 Series controllers. Observe the following guidelines when wiring a VMA18 controller.