Table 1 provides LED status indicator information for troubleshooting the VMA
18 controller.
Note: If you experience short
circuits in the 24 VAC power supply causing protective devices such as breakers or
fuses to trip, make sure that the power connections on the VMA are not reversed. The
most common cause of this problem is when the 24 VAC power supply on the VMA
is reversed but not reversed on a connected secondary device. Improper
wiring of this power terminal may cause a short circuit across the 24 VAC power
supply on -1 models.
| Problem | Possible cause | Correction | Verification | ||
|---|---|---|---|---|---|
| Controller is Off | Power at Primary of Transformer, 0V at Secondary | Transformer has tripped |
|
|
|
| Power at Primary of Transformer, 24 V at Secondary, 0V at Fuse/Breaker | Breaker/Fuse has tripped | ||||
| Configurable output - analog mode is invalid | 0–10 V output is set to 10–100%, but 0 V is at output terminals | Output is in protection mode - a state the analog portion of the configurable output goes into when it detects a wiring problem. The analog output is set to 0% regardless of the command whenever a wiring fault is detected | Power polarity mismatch between connected device and configurable output | Ensure polarities of ~24 V COM/OCOM match and that the connected end device uses the same polarity |
|
| 0–10V output has an undesirable offset of up to 1V | Common Reference is incorrect | OCOM terminal is not connected | Connect OCOM terminal of the configurable output to the common of the connected end device | ||