Sensor replacement and reuse scenarios - Metasys - MS-VMA1832-x - MS-VMA1826-x - Field Device - VMA18 VAV Modular Assembly

VMA1826/1832 VAV Controller Installation Guide

Product
Variable Air Volume > Modular Assemblies > VMA18 VAV Modular Assembly
Document revision
K
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-373

This section describes sensor replacement and reuse scenarios for replacing a VMA 1410, VMA 1415, VMA 1420, or the VMA controller with VMA18 controllers.

See Table 1 for a description of the most popular sensor models used with the VMA 1410, VMA 1415, VMA 1420, and the VMA controllers, the sensor replacement and reuse scenarios for that sensor model, and sensor replacement and reuse instructions.
Important: Complete all the steps in the Mounting section before following the instructions in this section.