Installation - Metasys - MS-VMA1832-x - MS-VMA1826-x - Field Device - VMA18 VAV Modular Assembly

VMA1826/1832 VAV Controller Installation Guide

Product
Variable Air Volume > Modular Assemblies > VMA18 VAV Modular Assembly
Document revision
K
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-373

Observe these guidelines when installing a VMA 18 Series controller:

  • Transport the VMA controller in the original container to minimize vibration and shock damage to the VMA controller.

  • Do not drop the VMA controller or subject it to physical shock.