SA Bus terminal block - Metasys - MS-VMA1630 - MS-VMA 1628 - MS-VMA1615 - MS-VMA1626 - Field Device - VMA16 VAV Modular Assembly

VMA1615/1626/1628/1630 VAV Controllers Installation Guide

Product
Variable Air Volume > Modular Assemblies > VMA16 VAV Modular Assembly
Document revision
K
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-217

The SA Bus terminal block is a brown, removable, 4-terminal plug with +15 VDC that fits into a board-mounted jack. Wire the removable SA Bus terminal block plugs on the VMA and other SA Bus devices in a daisy-chain configuration using 4-wire twisted, shielded cable as shown in Figure 1 . See Table 1 for more information.

Figure 1. SA bus terminal block wiring