The SA Bus terminal block is a brown, removable, 4-terminal plug with +15 VDC that fits into a board-mounted jack. Wire the removable SA Bus terminal block plugs on the VMA and other SA Bus devices in a daisy-chain configuration using 4-wire twisted, shielded cable as shown in Figure 1 . See Table 1 for more information.
Figure 1. SA bus terminal block wiring