Wiring - Metasys - MS-VMA1630 - MS-VMA 1628 - MS-VMA1615 - MS-VMA1626 - Field Device - VMA16 VAV Modular Assembly

VMA1615/1626/1628/1630 VAV Controllers Installation Guide

Product
Variable Air Volume > Modular Assemblies > VMA16 VAV Modular Assembly
Document revision
K
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-217
CAUTION
  • Risk of Electric Shock
  • Disconnect the power supply before making electrical connections to avoid electric shock.
ATTENTION
  • Risque de décharge électrique
  • Débrancher l'alimentation avant de réaliser tout raccordement électrique afin d'éviter tout risque de décharge électrique.
Important: Do not connect supply power to the controller before finishing wiring and checking all wiring connections. Short circuits or improperly connected wires can result in damage to the controller and void any warranty.
Important: Do not exceed the controller electrical ratings. Exceeding controller electrical ratings can result in permanent damage to the controller and void any warranty.
Important: Use copper conductors only. Make all wiring in accordance with local, national, and regional regulations.
Important: Electrostatic discharge can damage controller components. Use proper electrostatic discharge precautions during installation, setup, and servicing to avoid damaging the controller.

For information on configuring and wiring a BACnet/IP network, refer to the Metasys IP Networks for BACnet/IP Controllers Configuration Guide (LIT-12012458). For detailed information on configuring and wiring a SA Bus, refer to the MS/TP Communications Bus Technical Bulletin (LIT-12011034).