Commissioning Field Controllers - Metasys - MS-VMA1630 - MS-VMA 1628 - MS-VMA1615 - MS-VMA1626 - Field Device - VMA16 VAV Modular Assembly

VMA1615/1626/1628/1630 VAV Controllers Installation Guide

Product
Variable Air Volume > Modular Assemblies > VMA16 VAV Modular Assembly
Document type
Installation Guide
Document revision
K
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-217

To commission the VMA1615/1626/1628/1630 controller, use the following procedure:

  1. Download the control application to the controller using the Controller Configuration Tool (CCT). Refer to the Controller Tool Help (LIT-12011147).
  2. Commission the VAV Box. Refer to the Controller Tool Help (LIT-12011147).
  3. Perform airflow balancing on the VAV box. Refer to the VAV Balancing Tool Technical Bulletin (LIT-12011087) .
  4. Perform commissioning checkout procedures. Refer to the Controller Tool Help (LIT-12011147).

You commission controllers with the CCT software. The controller can be connected in one of four ways; either through NxE Passthru, MAP 4.2+/BACnet Router (Mobile Access Portal (MAP) Gateway at version 4.2 or above), through Bluetooth (using BTCVT), or Direct Ethernet connection to the controller. Refer to Controller Tool Help (LIT-12011147) for detailed information about commissioning field controllers.

Note:
  • The MAP Gateway serves as a replacement for the BTCVT, which is no longer available for purchase, but continues to be supported.