Entering balancing mode - Metasys - LIT-12011087 - NS-ATV7003-0 - NS-ATV7002-0 - NS-ATV7001-0 - NS-BTV7002-0 - NS-BTV7001-0 - Accessory - Handheld VAV Balancing Sensor/Tool - 6

VAV Balancing Tool and Network Sensors Technical Bulletin

Product
Variable Air Volume > Tools > Handheld VAV Balancing Sensor/Tool
Document number
LIT-12011087
Version
6
Revision date
2018-11-19

Before you begin

To enter balancing mode:

Procedure

  1. If you are using the handheld balancing tool, connect it to the Network Sensor associated with the controller you want to balance.
  2. Press and hold the Enter and Cancel buttons together for at least 5 seconds until the word Busy [BUSY] appears on the display.
    Note: The VAV Balancing Tool returns to normal operation after a certain period of inactivity, based on the Timeout Delay parameter in the Balancer Override module. The default Timeout Delay is 60 minutes.
  3. For Single Duct applications, see Balancing a single duct system. For Dual Duct applications, see Balancing a dual duct system.