Storing proxy credentials in the credential manager as a local user - Johnson Controls - Metasys - LIT-12012389 - Software Application - Software Licensing - 3.0

Software Manager Help

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
User Guide
Document number
LIT-12012389
Version
3.0
Revision date
2020-10-30

About this task

If credentials are required for the proxy server, you need to add them to the credential manager. To store your credentials in the credential manager, complete the following steps:

Procedure

  1. Go to Start>Control Panel>User Accounts>Credential Manager.
  2. Click Add a generic credential.
  3. In the Internet or network address field, enter SMProxyCredentials.
  4. In the User name and Password fields, enter your user name and password.
  5. Click OK.
    Note: If you have a local system account, then you need to directly log on to that machine with that local system account and then continue to work on the Software Manager.