Time Sheet Tab - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

The Time Sheet tab allows administrators to place time-of-day restrictions on user login. Users may log in to the system during any of the selected hours. Users are denied access when they try to log in during unselected hours (Figure 1). The Time Sheet tab is the same for both the Metasys local system user and the Active Directory service user. User access for an Active Directory service user is also controlled by an Active Directory service property called Logon Hours. See Authentication Process.

Figure 1. Time Sheet Tab

Table 1. Time Sheet Tab Parameter

Field

Description

Default Value

Required

Time of Day

Allows administrators to select times when users can access the system.

All hours selected

Yes