Security Toolbar and User Access Icons - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Table 1 describes the Security toolbar options, and Table 2 provides descriptions of the icons that appear next to a username.

Table 1. Security Toolbar

Icon

Description



Adds a new user to the Roles and Users tree. The User Properties dialog box appears.



Adds a new role to the Roles and Users tree. The Role Properties dialog box appears.



Adds a new Active Directory service user to the Roles and Users tree. The Add Active Directory User dialog box appears.



Marks the standard user account as disabled. Next time the user attempts to log in to the system, an account disabled message appears. An administrator must enable the account through the User Properties.

Note: Active Directory service users cannot be disabled in this manner. Active Directory Service administrator manages account accessibility.


Opens the System Privileges window.

Note: If you select apredefined role or predefined user, the System Access Permissions are read-only.


Saves the category-based permissions information.



Opens the Metasys Site Management Portal Help (LIT-1201793) , SCT: System Configuration Tool Help (LIT-12011964) , or the Open Application Server (OAS) Commissioning Guide (LIT-12013243) .

There is no Help system for the Security Administrator system. Information on the Security Administrator system is located only in Security Administrator System Technical Bulletin (LIT-1201528) (this document).

Note: A File Download dialog box may appear. To open the Help system, click Open.
Table 2. Icons That Indicate User Accessibility

Icon

Description



Standard access user account is enabled.



API Access account is enabled.



Tenant access user account is enabled.



Standard access Metasys user account is disabled (Account Disabled property check box selected). Metasys system access is suspended for standard access Active Directory service user. (Metasys Access Suspended property check box is selected).



Standard access Active Directory service user account is disabled in Active Directory service (Metasys Access Suspended property check box is cleared).



API Access Metasys local user account disabled (Account Disabled property selected). API access Active Directory service user account has Metasys system access suspended (Metasys Access Suspended property check box is selected).



API access Active Directory service user account is disabled in Active Directory service (Metasys Access Suspended property check box is cleared).



Tenant access Metasys local user account disabled (Account Disabled property selected). Tenant access Active Directory service user account has Metasys system access suspended (Metasys Access Suspended property check box is selected).



Tenant access Active Directory service user account is disabled in Active Directory service (Metasys Access Suspended property check box is cleared).