Security Database Backup and Restore for Metasys server - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Backing up and restoring the Security Database with SCT backs up and restores the Active Directory service users, Metasys local users, and roles for a Metasys server.

The following Metasys Active Directory service configuration information is stored in the Security Database and backed up or restored along with other Security data:

  • Active Directory Service Authentication Enabled or Disabled
  • Windows Workstation SSO Enabled or Disabled
  • Login Page Default Domain Selection
  • Active Directory Service Service Accounts

Settings from the backup replace existing settings on the targeted device during a restore operation.