Summarized Tab - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

When you are viewing user system privileges, select the Summarized tab to view all system privileges assigned to the user either directly or by a role. This tab includes the same information as the Role/User Assigned tab, but you cannot add or remove privileges by using the Summarized tab. This tab does not appear when viewing role system privileges.