Role/User Assigned Tab - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

The Role/User Assigned tab in the System Privileges for User Operator dialog box shows only those system level permissions directly assigned to the role or user.

Figure 1. System Privileges User Assigned Dialog Box

Table 1. Role/User Assigned Tab Parameters

Field

Description

Default Value

Available Privileges

Displays the available System Privileges that may be assigned to a user or role.

All Available Privileges

Assigned Privileges

Displays the System Privileges assigned to the user or role.

Note: For Metasys Release 7.0 or later, assigning the System Configuration Tool privilege through the SMP does not grant the user access to the application. The SCT user system privileges are maintained and accessed separately through the SCT UI.

Add

Moves the selected Privileges from the Available (System) Privileges list box to the Assigned (System) Privileges list box. Privileges are then assigned to the user or role.

Remove

Moves the selected Privileges from the Assigned (System) Privileges list box to the Available (System) Privileges list box. Privileges are then removed from the user or role.