Actions for Metasys UI Users - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Table 1 lists the actions that users can perform in the Metasys UI with the corresponding required privileges for those actions. For all of the below actions, you must have authorization category permission.

Table 1. Actions and Corresponding Privileges for Metasys UI Users
Metasys UI Action Authorization Permission Required

Adjust

Operate Permission (Authorization Category-Based)

You must have authorization category permission for the point that you are adjusting.

Override

Intervene Permission (Authorization Category-Based)

You must have authorization category permission for the point you are overriding.

Release

Intervene Permission (Authorization Category-Based)

You must have authorization category permission for the point you are releasing.

Take Out of Service

Put Back in Service

Diagnostic Permission (Authorization Category-Based)

You must have authorization category permission for the point you are taking out of service or putting back in service.