Account Removal During Uninstall - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Metasys servers - ADS/ADX/OAS

When you uninstall a Metasys server, the default SQL server login accounts are removed, even if you choose to retain the databases. This means that you must reset the passwords after you reinstall the server.

SCT

When you uninstall the SCT, the archive database accounts are maintained. There is an option to remove the SCT database and SQL Server login accounts during the SCT uninstall.