Users Tab - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

The Users Tab allows administrators to assign users specific roles (Figure 1). The following example shows that Active Directory service for use by the Metasys system is enabled with a defined set of Metasys local system users and Active Directory service users.

Figure 1. Users Tab

Table 1. Users Tab Parameters

Field

Description

Default Value

Available Users

Users Not Assigned to the Role

All Available Users

Assigned Users

Users Assigned to the Role

Add

Moves the users from the Available Users list box to the Assigned Users list box. Once in the Assigned Users list box, the role access privileges are granted.

Remove

Moves the users from the Assigned Users list box to the Available Users list box. Once in the Available Users list box, the role access privileges are removed.

Note: You cannot remove the MetasysSysAgent user from the ADMINISTRATOR role.