Domain List Rules - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

The list of domains that appear on the Metasys login screen depends on the following:

  • If more than one service account is defined, the domain list displays the domains of the service accounts.
  • If only one service account is defined, the domain list is based on the list of users added to the Metasys system. In other words, the domain list changes as users from different domains are added and removed from the Metasys system.