- To grant permission for a user for a particular category, tap or click on the desired permission column. A white check mark on a green circle appears. To remove a user-assigned permission, click the icon.
- Tap or click SAVE to save your settings and exit the Category Access tab, or tap or click CANCEL to exit the tab without saving your changes.
The following table lists the available permissions.
Important: Some
of the available permissions listed below are applicable to SMP only. See the notes
in the Description column for further details.
Name | Description |
---|---|
No Access | The No Access column shows the combined settings for No Access from all of the user's roles and is disabled when assigning permissions to a user. |
View | Gives the user the
following privileges:
Important: To snooze an alarm in the
Alarm Bar, the user must have View permission and Manage Item
Events permission. The Alarm Bar is a feature in SMP
only.
|
Advanced View | Gives the user the
same privileges as the View permission, in addition to the
capability of editing the advanced attributes for users with edit
privileges. When not selected, the Advanced option in all item views
(for example, Focus view) is disabled. Note: This refers to SMP only. Metasys UI views do
not have an Advanced View option.
|
Operate | Gives the user the
following privileges:
|
Intervene | Gives the user the
following privileges:
|
Diagnostic | Gives the user the
following privileges:
|
Manage Item Events | Gives the user the
following privileges:
Note: Applies to category-based events and allows the
user to display an alarm in the Alarms Window (also referred to
as Metasys - Events and Alarm Bar.) The Alarm Bar is a feature
in SMP only.
|
Manage Energy | Gives the user the
following privileges:
|
Modify Items | Gives the user the
following privileges:
Note: When users modify items, they can only set the
Authorization Category property of a modified object to a
category for which they have Modify Items access
permission.
|
Configure Items | Gives the user the
following privileges:
Note: When users create objects, they can only set
the Authorization Category property to a category for which they
have configuration access permission. The functionality to
create objects is available in SMP only.
|
Note: There are slight
layout differences on a smartphone. For example, select User Details, Account
Settings, Timesheet, and
Category Access from the drop-down menu
in the upper-left of the phone screen.