Setting Password Account Policies - Metasys - LIT-1201528 - General System Information - Metasys System - 12.0

Security Administrator System Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-1201528
Version
12.0
Revision date
2022-08-05

Procedure

  1. Select the user to configure.
  2. On the Edit menu, click Properties. The User Properties dialog box appears. See Figure 1.
  3. Select the Account Policy tab.
  4. Select options using Table 1 (Metasys local users) or Table 2 (Active Directory service users).
  5. Click OK.